Advanced Reporting and Dashboards licensing options

For the Advanced Reporting and Dashboards Module, only a single license is required. For more information on licensing, see License keys.

NOTE: Requires at least one Power Operation Server and one Client Access license (either thick client or web client). No additional PME client or device licenses are required for this module as the Power Operation Server and Client Access licenses cover the device licenses (i.e. PME DLs) and client connectivity to the reports and dashboards.