Smart Connector Requirements

Smart Connector requires a Microsoft SQL Server. Smart Connector integrations are only supported with Power Operation 2021 and above.

Supported Windows operating systems
  • Windows 10 (64-bit only)

  • Windows Server 2021 R2

  • Windows Server 2016

  • Windows Server 2019

Supported SQL Server versions used with Smart Connector
  • Microsoft SQL Server 2012 Express/Standard/Enterprise/Business Intel

  • Microsoft SQL Server 2014 Express/Standard/Enterprise/Business Intel

  • Microsoft SQL Server 2016 Express/Standard/Enterprise/Business Intel

Hardware Requirements

Physical and virtual machine CPU and RAM requirements for Smart Connector will vary based on a number of factors, including:

  • Number of tags being shared with the third-party system.

  • Data exchange rate of tags being shared with the third-party system.

  • Specific third-party system end point requirements.

As a result, CPU and RAM requirements will vary by project.