Power Operation Tool Suite

notice

INOPERABLE SYSTEM

Ensure that you have received training and understand the importance of the Power Operation productivity tools and workflows.

Failure to follow these instructions can result in overly complex projects, cost overruns, rework, and countless hours of support troubleshooting.

NOTE: Power Operation is built on Power Operation Studio and includes productivity tools that are designed and optimized to create the tags you need to configure power-based SCADA projects. If you have prior experience using Power Operation Studio, do not rely exclusively on Citect tools to build a SCADA project.

 

Deploy projects faster with the Power Operation Tool Suite, including tools that are unique to Power Operation and critical to project success.

The suite includes:

  • Simple SCADA Project Setup
  • Centralized SCADA Project Deployment
  • Power Operation Studio
  • Power Device management
  • IO Devices Comms Optimization

The following Power Operation features are supported only using Power Operation tools and workflows:

  • HTML5 built-in graphics, alarms, and waveforms
  • Event Notification Module
  • Interoperability with Advanced Reporting (specifically ETL for PME)
  • Interoperability with EBO (specifically PO EWS implementation for EBO)
  • LiveView
  • Basic Reports
  • One-line configuration
  • Power Operation power graphics libraries (genies)
  • I/O Device Manager (both UI and Excel)
  • The ION and Power Modbus drivers are complex to setup without the use of Power Operation tooling