Waveform file share access and permissions

Waveforms are stored in a file share repository on the Power Operation Server.

The following waveform file share permissions are required:

  • The account running Citect on Power Operation Server requires Full permission (Read/Write/Modify)
  • Windows user accounts that are used to log-into remote machines using HTML5 web clients require Read Only permission.
  • Windows user accounts must be linked to Power Operation user roles that allow Remote Procedure Call (RPC).
  • NOTE: This is required to get a list of waveforms from the Server.

Architecture #1: HTML5 Web Client

Architecture #2 Power SCADA Anywhere