Backing up the Power Operation passwords and device profiles
This section includes information on backing up passwords and device profiles. Because Power Operation passwords and device profiles cannot be automatically backed up, you must back them up manually.
NOTE: The encrypted file that stores this password cannot be transferred from one machine to another, so it is very important that you store this password somewhere secure where it can be retrieved.