Activating a license
Activate a license to enable the use of your system after a new install, an upgrade, or a migration. Activate licenses to enable features, such as software modules, or additional monitoring devices.
You can activate licenses online, directly from the Power Operation (PO) server if it has an Internet connection. You can also activate licenses offline, from an alternate internet-connected computer or smartphone. In both cases, you use the License Configuration Tool to activate licenses.
NOTE: You must have a valid Activation ID to activate a license.
To activate a license online:
- On the PO server, open the License Configuration Tool, and click Activate License. A message box is displayed.
- Read the information and click OK. The Activate License page opens.
- On the Activate License page, enter the Activation ID, and then click Activate.
- Close the License Configuration Tool.
NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by
clicking Start
on the taskbar and choosing
Schneider Electric > Power Operation License Configuration Tool.
NOTE: By default, the activation method is set to Online.
The license appears in the License Configuration Tool.
To activate a license offline:
- On the PO server, open the License Configuration Tool, and click Activate License. A message box is displayed.
- Read the information and click OK. The Activate License page opens.
- On the Activate License page, set Activation method to Offline.
- In the Initiate section, enter the Activation ID and select the location to save the activation request file. Click Download. The activation request file
capabilityrequest.bindownloads to the selected location. - Copy the
capabilityrequest.binfile to a computer or a web-enabled device, such as a smartphone with Internet access. - On the Internet-connected computer or device, open a Firefox or Chrome browser.
- Browse to the Offline Licensing Web Portal (https://schneider-electric.flexnetoperations.com/flexnet/operationsportal/logon.do).
- Log in using the activation ID.
- Click the Devices drop-down and then click Offline Device Management. The Offline Device Management window opens.
- On the Offline Device Management page, click Choose File, and then select the
capabilityrequest.binfile, and click Upload. The Download my License Response File window opens. - In the Download my License Response File window, click Download to save the
capabilityresponse.binfile. - Copy the
capabilityresponse.binfile to the PO server computer. - On the PO server, open the License Configuration Tool, and click Activate License. A message box is displayed.
- Read the information and click OK. The Activate License page opens.
- On the Activate License page, set the Activation method to Offline.
- In the Complete section, select the location of the
capabilityresponse.binfile, and click Activate. The license appears in the License Configuration Tool. - Close the License Configuration Tool.
NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by
clicking Start
on the taskbar and choosing
Schneider Electric > Power Operation License Configuration Tool.
NOTE: By default, the activation method is set to Online.
NOTE: Internet Explorer is not supported.
TIP: If you are using a smartphone, try using a USB cable to copy the file.
NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by
clicking Start
on the taskbar and choosing
Schneider Electric > Power Operation License Configuration Tool.
NOTE: By default, the activation method is set to Online.