Restore the databases from the old system
Restore the backed-up databases to the new PME system at their installation location.
To restore copies of the backed up PME databases into the new PME system:
- In SQL Server Management Studio, right-click Databases and then click Restore Database.
- Click Device and then click the ...(ellipsis) button.
- Click Add.
- In the Locate Backup File dialog, navigate to the location where the backup database files are stored and enter the database name in the File name field.
For example: - Click OK.
- Make sure that Restore is checked:
- Click on the Files tab on the upper left of the window, select Relocate all files to folder, and then select the location for restoring the database:
- Select the default location for the PME databases. For example:
- Click OK.
- Repeat Steps 1 to 9 for the remaining database files (ION_Data and ION_Network).
The following image shows the restored databases: