Software prerequisites

The following software components are required for the operation of Power Operation. These software components will be installed during the Power Operation installation:

  • NET Framework 4.8
  • NET Core 6 (6.0.9) - Windows Desktop Runtime, ASP.NET Shared Frameworks, Runtimes, and Windows Server Hosting
  • IIS URL Rewrite Module 2
  • WebView2 Runtime
  • Microsoft Visual C++ 2008 Redistributable
  • Microsoft Visual C++ 2010 Redistributable
  • Microsoft Visual C++ 2012 Redistributable
  • Microsoft Visual C++ 2015-2022 Redistributable
  • Visual FoxPro OLE DB Provider