Add setpoints and delays

Any time you change setpoints, you should immediately restart the project. Otherwise, setpoints will not be properly read (they will be truncated and either rounded down or up to a whole integer).

NOTE: Before you enter setpoints and delays, ensure that you have configured the Alarm Server so that Publish Alarm Properties is set to TRUE.

There are 2 ways to add setpoints and delays for analog alarms:

  • From the Analog Alarms window (accessible from the Project Explorer or Project Editor screens), you can type the setpoint and delay values for each alarm.
  • In Power Operation Runtime, you can edit setpoints/delays that were set by the method previous.

Also, set the following parameter to allow persisting of alarm parameters at runtime:

[Alarm] UseConfigLimits = 1