Set up an alarm based on an enumeration
To define an enumeration in the Profile Editor, see Define an enumeration.
An example of an enumeration alarm is:
- 0 = unknown
- 1 = good
- 2 = warning
- 3 = alarm
To add an alarm that is based on an enumeration:
- Open the analog alarm in Power Operation.
- To alarm on states 0, 2, and 3:
- Set Low = 1 (if the value < 1, the alarm indicates an unknown state)
- Set High = 1 (if the value > 1, the alarm indicates a warning)
- Set High High = 2 (if the value > 2, the alarm indicates an alarm)
- In the Category field, ensure that the correct alarm level is entered (_PLSALM_HIGH, _PLSALM_MEDIUM, _PLSALM_LOW, _PLSALM_EVENT).
- Replace the alarm.