Overview
This application provides remote, continuous monitoring of the thermal conditions of MV substations equipped with Easergy TH110 temperature sensors and Easergy CL110 environmental sensors. Thermal monitoring can help you find exceptional conditions in the substation equipment, such as overloads or faulty power connections of cables, busbars, circuit breakers, or transformers. In addition, this application can monitor the environmental conditions, ambient temperature and humidity, inside the substation and switchgear cubicles. You can see temperature data in real-time, analyze historical trends, and receive alarms and notifications. Any applicable Power Operation power monitoring features can be used with the substation monitoring data.
For more information on the value of Continuous Thermal Monitoring see the EcoStruxure Power Digital Applications for Large Buildings & Critical Facilities Design Guide on www.se.com or the Schneider Electric Community.
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.