Prerequisites
The following is required to set up the Thermal Monitoring of MV Substations application in Power Operation 2022:
- Power Operation 2022 must be installed and commissioned.
- The TH110 and CL110 sensors, the ZBRN32 access points, and the SMDs in the substation must be configured, connected, and communicating.
NOTE: This application supports SMD v4.0 and v3.0. SMD v2.0 is not supported.
- The SMDs must be accessible from the Power Operation server by Ethernet.
- You must know the IP address of the SMDs.
NOTE: If you are using Power Operation 2022 with Advanced Reporting and Dashboards and want to set up dashboards to display substation data, refer to the Thermal Monitoring of Medium Voltage (MV) Substations section in the Power Monitoring Expert System Guide.