Export and import One-Time Password settings
You can copy and use one-time password settings on multiple server computers.
NOTE: When you import password settings into another server, you will overwrite any password settings that already exist there. You are not simply adding the new password settings to the existing ones.
To copy and use one-time password settings on multiple server computers:
- In the Application Configuration Utility: click the Security drop down and then click One-time Password.
- Click Export. A file named
ExportedOTPConfiguration.xmlis generated. You can rename it if you wish. Save it where you can access it from other servers, or copy it to a portable drive. - From a server to which you want to import the password settings, click Import. You are prompted for a location.
- Browse to the location where you placed the XML file. Click Open and accept the XML file.