Before adding I/O devices
Have a copy of each device’s communication protocol and IP address. You will need to enter this information when you add the devices.
NOTE: You can use IPv6 IP addresses – including IPv6 shorthand – for TCP/IP level drivers.
For each cluster and the appropriate servers for this project (see the Plant SCADA help file for details)
For each cluster :
- From the I/O Device Manager, under System Devices, click Cluster Setup and then click Next.
 - At the Enter Instance Information screen, a cluster name displays. Click Next.
If there are multiple clusters, the Select cluster screen displays
 - Choose the cluster you want to set up and then click Next.
If there are multiple I/O servers, the Select I/O Servers screen displays.
 - Select an I/O Server. (Optional) If you are developing a redundant system:
 - Check Supports Redundancy and select the I/O servers to which you want to add the device.
 - Click Next.
 - At the Ready to perform action screen, click Next.
 - If you have more than one cluster to add, repeat steps 3 through 6 for each cluster.
 - When you are finished adding clusters and I/O servers, you return to the I/O Device Manager welcome screen.