Define multiple devices using a CSV file
I/O Device Manager makes it easy to create a Power Operation project. Use this tool to make either single or bulk additions, updates, and deletions to the Power Operation device database.
Valid communication protocols are:
- DNP3 Serial
 - DNP3 Ethernet
 - Modbus/RTU Gateway
 - Modbus TCP
 - ION
 - ION/Gateway
 - IEC60870-5-104 TCP
 - IEC61850