Delete a custom tag

You can delete any custom tag that is not associated with a device type.

  1. If the tag is associated with a device type, you must first deselect the tag:
  2. Change the option to Edit Existing and display the tag you want to delete.
  3. Click Display Associated Device Types to display all device types that include this tag. Make a note of the device types.
  4. Return to the Add/Edit Device Type screen. For each device type listed, deselect the tag that you want to delete.

Continue deleting the tag:

  1. Open the Add/Edit Custom Tags screen.
  2. In the Custom Tag Options box, click Delete Existing.
  3. From the drop-down menu, choose the tag you want to delete.
  4. Click Delete.
  5. Click Yes to confirm the deletion.
  6. Click Save to save the change, or click Save & Exit to save changes and close the screen.