Edit a custom tag

You can edit any custom tag.

To edit a tag:

  1. Open the Add / Edit Custom Tags screen: from the Add / Edit Device Type screen, click Add / Edit Custom Tags.
  2. In the Custom Tag Options box, click Edit Existing.
  3. You can change any of the tag attributes. (This does not change the tag’s assignment status; if it is selected for a device type, it does not move back to the IEC Tags list.)
  4. Click Save to save changes, or click Save & Exit to save changes and close the screen.