Printing the .CSV file

For each device type, device profile, or project, you can create and print a CSV file that includes the following data:

Type of File

Data Included

Device Type

tag descriptions, IEC tag names, type, and address

Device Profile

tag descriptions, IEC tag names

Project

data profiles and custom tag names included in the project

To create and print the CSV file:

  1. Display the device type, profile, or project for which you want the file. For example, to create a CSV file for the Sepam 42 Full device profile, select the Create Device Profiles tab and choose Sepam S42 Full from the drop-down list.
  2. Click File > Create CSV File.
  3. In the Save As window, choose a location for the file and optionally rename it. Click Save.

    The file is created in the location you specified.

  4. View and print the file in Microsoft Excel.