Reviewing Genie Configurations

Use the One-Line Configuration Utility to review genie configurations before you compile your project.

If you are upgrading from an earlier version:

  • Run Update Pages in the Graphics Builder.
  • Create the pages.

Errors ( ) and warnings ( ). You must correct errors; otherwise, you may not be able to compile, and the animation will not work. Although you might not need to correct warnings, you should review them to ensure that their settings are correct.

TIP: When you hover over an error or warning icon, a tooltip tells you what is wrong with the genie.

To launch the One-Line Configuration Utility:

  1. Make sure you are viewing the system for which you want to view information.
  2. In Power Operation Studio, click Launch the Single Line Configuration Utility .
  3. Click OK to the message that displays.
  4. The first time you load the utility, a large system could take a couple of minutes to load. After that, it should load within a minute.

    There are 2 tabs:

    • Use Genie Configuration to:
      • View genie types, along with their states (normal, warning, error) and their properties
      • Repair genies that are part of a version 7.30 or later project:
        • Corrects incorrect breaker, source, meter, transformer, and Sim source numbers
        • Corrects invalid line active when a connected busbar has a valid line active
      • Repair and upgrade genies that are part of a project from a version earlier than 7.30
        • Renumbers ALL breaker, source, meter, and Sim source numbers
        • Corrects invalid line active when a connected busbar has a valid line active
        • Reassigns ALL valid busbars
    • Use Color Configuration to assign colors to sources.

     

    The Genie Configuration pane contains the following information:

    Field

    Description

    Projects

    Default: the project selected in the Power Operation Studio

    Show By

    Type: Information is sorted first by genie type, then by page. This option is useful when you want to see all genies of a certain type together, regardless of where they are in the drawing pages.

    Page: Information is sorted first by page, then by genie type. This option is useful when you want to see all genies on a certain page.

    Advanced Properties

    Check this box to view the basic information plus any additional information relevant to that genie type.

    State Filters

    Check the individual boxes for how you want to view information. For example, you might only be interested in viewing genies that have error states. This option controls only the genie information in the right-hand pane.

    Genie Types tree

    Types are: breakers, busbars, meters, sources, and transformers

    Genie Information grid

    Columns of information display:

    In the Basic (default) view: the most used information

    If you click Advanced Properties, you see the basic information, followed by all the information known about the genie(s) you are viewing.

    Repair—Upgrade Project

    Check this box to cause the repair feature to repair the entire project.

    Use this feature only to upgrade projects that are earlier than Power Operation 2022. This option repairs the entire project, renumbering all busbars, breakers, meters, duplicate Sim sources, and sources. Additionally, busbar line active states are used to determine meter and source line active states.

    DO NOT perform Repair—Upgrade Project more than once, and do not perform it on a Power Operation with Advanced Reporting and Dashboards project.

    Repair

    This feature attempts to repair errors and warnings.

For specific information about each type of genie, click a link below: