Adding Menu Items for LiveView Data Tables

Using the names of real-time data table views that you saved earlier (see Create Real-Time Data Views), you need to add a Menu Configuration item for each saved view.

In Power Operation Studio, click Visualization > Menu Configuration.

The following would save a view named "BasicReadingsSummary," with "localhost" used to indicate that LiveView is running on the Power Operation server. Use the PLS_LiveViewDsp cicode function to display your saved view in the operator HMI.

  • Level1: Applications
  • Level 2: LiveView
  • Level 3: Basic Readings
  • Menu Command: PLS_LiveViewDsp("localhost", "BasicReadingsSummary", "BasicReadings")
  • Symbol: PLS_Icons.Reports_16x16

Add the corresponding information for each saved real-time data table view you wish to see in the Power Operation Runtime.