Busbar Information

The most commonly used information about the busbar genie displays by default.

When the Advanced Properties box is selected, the table expands to include everything that is known about the selected busbar(s).

Basic busbar information includes:

Column

Description

State

Normal (), Warnings (), or Errors (). See the following table for explanations of errors.

Page

Name of the page on which the genie is found (displays only from the folder level).

ID

This is the busbar number, assigned when adding it to a page of a one-line.

Busbar Errors

Before you use the drawing, correct all errors; otherwise the project might not compile and the animation will not work.

Errors that you might see for busbars are:

State

Solution

Errors ()

Busbar number must be a number greater than 0.

The busbar number is missing, or it is less than or equal to 0. Add or change the busbar number.