Source information

The most commonly used information about the source genie displays by default. A source genie is required and must be properly configured.

When the Advanced Properties box is checked, the table expands to include everything that is known about the selected source(s).

Basic source information includes:

Column

Description

State

Normal (), Warnings (), or Errors (). See the following table for explanations of errors and warnings.

Page

Name of the page on which the genie is found (displays only from the folder level).

ID

This is the meter number, assigned when adding it to a page of a one-line.

Busbar

The number of the source that powers the connected busbar.

Line Active

The Cicode expression (such as MyTag1 > 0) that determines when the source detects power on the busbar.

Source Errors and Warnings

Before you use the drawing, correct all errors; otherwise the project might not compile and the animation will not work.

Warnings indicate settings that might be incorrect. Verify that the settings indicated by the warnings are what you want.

Errors and warnings that you might see for sources are:

State

Solution

Errors ()

Source number must be a number greater than 0 and unique.

The source number is missing, or it is less than or equal to 0. Add or change the source number.

Busbar number must be a number greater than 0 and unique across sources.

The busbar number is missing, or it is less than or equal to 0. Add or change the busbar number.

Busbar number must exist (busbar may link to a Busbar, transformer, or breaker)

At least one busbar must be linked to this source.

Warnings ()

Line Active should be present.

Line Active should be entered so the source can detect power on the busbar.