Adding the Tag Viewer page menu item

The Tag Viewer displays in the graphics page during runtime. Use the Tag Viewer to view details about equipment. This screen provides the status of project tags.

To add the Tag Viewer to a project graphics page:

  1. In Power Operation Studio, click Visualization > Menu Configuration.
  2. In the Menu Command line, add the Cicode method that will open the page:
  3. PLSPageDisplay("PLSTagView")

When viewing the Tag Viewer in runtime, as long as the screen resolution is one that Power Operation supports, the view will be correct.

For information about viewing tags, see Tag Viewer.