Duplicate LiveView template

You can duplicate an existing template, including predefined templates. The duplicated template will not be locked, allowing you to edit and save it as a different template.

  1. Open LiveView Template Editor.
  2. In Runtime mode, click the menu links that have been set up when you created the graphics page (see Create menu item for LiveView page). In the PLS_Example project, there is a tab for LiveView.
  3. Highlight the name of the template that you want to duplicate. The template displays.
  4. Click Duplicate (on the top of the left-hand pane).
  5. The duplicate template is added to the list. It has the same name of its original template, appended with "Copy."

  6. Change the name of the duplicated template to differentiate it from its original.
  7. Make the desired changes and then click Save to save them.