Configuring the Email Server
To send notifications using email, you must configure the email server.
To configure the email server:
- Opening Notifications Settings
- Click Settings and Diagnostics, and then click Email Setup.
- Enter the email server settings.
Refer to the following table for a description of the email server values:
| Email Server Setting | Description |
|---|---|
| SMTP Server | The server name or IP address of the provider. |
| From Address | Appears in the “From” field of the sent email. |
| User Name | Login for the SMTP Server, if required. |
| Password | Password for the SMTP Server, if required. |
| Enable SSL | Indicates whether the email is sent using Secure Sockets. |
| Service Port | The port number on the SMTP host. The default value is 25. |
| Timeout | The duration (in seconds) to wait before not sending an email. |
| Retries | The number of unsuccessful send attempts are made before the email is not sent. |
| Backoff | The delay (in seconds) between retries. |