Tag naming convention
Tag names cannot exceed 79 characters. Use a backslash as a separator between tag parts. Tags are constructed in this manner:
EquipmentName\Logical_Node\Data Object\Data Attribute (may have more than one)
For detailed information on tag syntax, see Tag Name Syntax in Plant SCADA Help.
The following table lists the main categories for the common IEC 61850 logical nodes. After the table, the most commonly used category (Mxxx: metering and measurement) is described.
| 
                                                         Category Name  | 
                                                    
                                                         Description  | 
                                                
| 
                                                         Axxx  | 
                                                    
                                                         automatic control; e.g., ATCC (tap changer), AVCO (voltage control)  | 
                                                
| 
                                                         Cxxx  | 
                                                    
                                                         supervisory control; e.g., CILO (interlocking), CSWI (switch control)  | 
                                                
| 
                                                         Gxxx  | 
                                                    
                                                         generic functions; e.g., GGIO (generic I/O)  | 
                                                
| 
                                                         Ixxx  | 
                                                    
                                                         interfacing/archiving; e.g., IARC (archive), IHMI (HMI)  | 
                                                
| 
                                                         Lxxx  | 
                                                    
                                                         system logical nodes; e.g., LLNO (common), LPHD (physical device)  | 
                                                
| 
                                                         Mxxx  | 
                                                    
                                                         metering and measurement; e.g., MMXU (measurement), MMTR (metering), MSTA (metering statistics), MSQI (sequence and imbalance), MHAI (harmonics and interharmonics)  | 
                                                
| 
                                                         Pxxx  | 
                                                    
                                                         protection; e.g., PDIF (differential), PIOC (instantaneous overcurrent or rate of rise.), PDIS (distance), PTOV (time-overvoltage)  | 
                                                
| 
                                                         Rxxx  | 
                                                    
                                                         protection related; e.g., RREC (auto reclosing), RDRE (disturbance)  | 
                                                
| 
                                                         Sxxx  | 
                                                    
                                                         sensors, monitoring; e.g., SARC (arcs), SPDC (partial discharge)  | 
                                                
| 
                                                         Txxx  | 
                                                    
                                                         instrument transformer; e.g., TCTR (current), TVTR (voltage)  | 
                                                
| 
                                                         Xxxx  | 
                                                    
                                                         switchgear; e.g., XCBR (circuit breaker), XCSW (switch)  | 
                                                
| 
                                                         Zxxx  | 
                                                    
                                                         other equipment; e.g., ZCAP (cap control), ZMOT (motor)  | 
                                                
The following example illustrates the IEC 61850 tag for current A:
EquipmentName\MMXU1\A\PhsA
                                        
where:
M = the category
MXU = measurement of currents, voltages, power, and impedances
1 = the instance (there could be multiple MMXU tags)
A = the data object, current
PhsA = the attribute that further defines the data object, phase A
All of the tags that are currently used in the system can be viewed from the Profile Editor > Define Device Type Tags tab. Click Settings > Display Advanced Properties to display the full tag names.