Associating datapoints with profiles
Use Profile Studio to manually or automatically associate profiles with datapoints. For more information, see Datapoints with associated profiles.
To associate profiles with datapoints
- In the main menu, click the Auto assign Profiles button
. - In the Automatic Profiles Association dialog, under Datapoints source, choose one of the following:
- Project
- Datagrid
- Selection
- Under Settings, enable or disable the following:
- Assign already assigned datapoints
- Assign unassigned datapoints
- Unassign already assigned datapoints
- Click OK.
To manually associate a profile with one or more datapoints
- In the Datapoints tab, select one or more datapoints.
- Select the profile from the Configuration pane Profiles tab.
- Do one of the following:
Click the
button.Drag the profile and drop it onto the datapoint in the list.
To unassign a profile with one or more datapoints
- In the Datapoints tab, select one or more assigned datapoints.
- Click the
button.