Profile Studio setup
During setup, you can determine whether to configure your devices for EcoSUI and EcoGTW by choosing EPAS, or for Power Operation by choosing EPO. This defines which HMI is used with the stated IP address.
-
If Power Operation Studio is installed on the same system as Profile Studio, EPO will be selected by default.
-
If EcoSUI is installed on the same system as Profile Studio, EPAS will be selected by default.
Project data in your Profile Studio project comes from your SCD file, which is provided or generated by EPAS-E or another program. You can import an SCD file during setup.