Creating virtual datapoints
In Profile Studio, create formulas using datapoints as inputs. These are called virtual datapoints.
NOTE: This feature is only available for an EPAS system.
To create virtual datapoints
SPS2DPS is a DPS type created from an SPS.
-
Select a location in the Navigation pane below the root node.
-
In the Virtual datapoints tab, right-click and choose one of the following from the context menu:
-
SPS
-
SPC
-
DPS
-
DPC
-
MPS
-
MV
-
SPS2DPS
The virtual datapoint appears in the Virtual datapoints tab.
To define virtual datapoint inputs and formulas
-
Select your virtual datapoint.
-
In the Configuration pane Virtual datapoints tab, click the Edit inputs button.
-
In the Information dialog, click OK.
-
In the Datapoints tab, select a datapoint with an associated profile (in black).
-
Click the
button. The datapoint is associated with the virtual datapoint you created. -
Click the Edit formula button.
-
In the Virtual datapoint editor, define a formula to calculate the virtual datapoint's value from the associated datapoint.
-
On the Signal quality drop-down list, select one of the following:
-
AlwaysValid: The formula is always valid.
-
ValidIfAllSignalsAreValid: The formula is valid when all signals (input) are valid.
-
ValidIfOneSignalIsValid: The formula is valid when one of the signals (input) is valid.
-
Click OK.