SCADA Projects
SCADA projects are repositories that hold the configuration information for your system that includes information such as servers and other system components, I/O devices, tags, alarms, and graphic pages that are used to build a runtime system, and Cicode/CitectVBA.
The configuration for a runtime system can be spread across multiple projects depending upon the scale of operations. Small, simple operations may require only a single project that houses all components required for runtime. For larger, complex operations or multi-site operations, several projects can be created based on specific plant areas, engineering processes or libraries, which are “included” together to form a single merged configuration used at runtime.
This section includes the following project-related topics:
- Restore a project
- Use the Migration Utility
- Before you add a project
- Add a project using Project Setup
- Compile a project
- Backup a project
In the Plant SCADA help file ( ..\Program Files (x86)\Schneider Electric\Power Operation\v2022\bin\Help\SCADA Help), see also:
- Plant SCADA Projects for information about the components that make up a project. This topic also discusses physical layout, requirements such as architecture and security, and project design.
- Project Types for information on preparing for a project.
For more information, visit the AVEVA Plant SCADA Forum.