Reuse projects created in the Profile Editor

You can create a project that can subsequently be reused for different installations.

To save and then reuse projects:

  1. Export the project from the Set Up Project tab of the Profile Editor.
  2. Click the folder icon beside the Export link:
  3. Copy the file (Equipment.profiles) that displays. If you need to use this file to another computer, you can move it to a portable drive.
  4. On the server computer, paste Equipment.profiles to the location, where:

    [Drive Letter]: The drive on which you installed the server

    The Application Data and ProgramData folders are not hidden (set the folder view for “view hidden folders”)

    [Project]: The name of the project you are creating; you must have already added this project to Power Operation.

  5. Be sure you have created the files described in Before you add a project.