Waveform Extractor scan interval settings

The Waveform Extractor scans for new waveforms once every five minutes. There is a 50 millisecond delay:

  • After scanning each device
  • After each new file is downloaded

These intervals can be increased or decreased based on your needs.

To change the cycle time settings:

  1. Close Power Operation Runtime.
  2. Navigate to .:\Program Files (x86)\Schneider Electric\Power Operation\v2022\Applications\Waveform Extractor\Service. In a text editor, open the appsetting.json file.
  3. Increase or decrease the following settings:
  4. Settings Details
    delayInBetweenRuns Adds a delay in between each run in order to scan all devices for new waveforms. Set the desired interval using the "HH:MM:SS" format.
    delayInBetweenDeviceMs Adds a delay in milliseconds in between scanning each device for a list of current files on the device.
    delayInBetweenFilesMs Adds a delay in milliseconds in between downloading each file from a device.
  5. Open Power Operation Runtime.
  6. In Task Manager, on the Details tab, confirm that WaveExtractorService.exe is running.