Configuring a Waveform Extractor project

You can use the Waveform Extractor to download waveforms from meters using FTP or SFTP protocols. To view Comtrade files acquired using FTP or SFTP protocols within the WebHMI, you must have an associated alarm with a matching timestamp.

If the device is unable to reliably generate alarms within +/- 500 milliseconds of the Comtrade timestamp, use the following steps to create an alarm that meets these requirements:

You can define the variable tags that will be referenced by the timestamped digital alarms.