Managing CAE models
A model is a representation of a program or device in the control system and its objects, such as a tool, utility, or an application function block. You can create models in CAE to assign them to roles.
A model includes security capabilities to create:
-
Permissions for components in a model.
-
Objects for the permissions.
-
Actions for each permission.
-
Parameters for Device Specific Settings (DSS) (optional).
Recommendations:
-
Assign roles only the essential privileges needed to perform their job.
-
Follow user account management tasks as described by your organization or contact your network administrator.
Showing MODELS tab
The MODELS tab is hidden by default and can be enabled using a security administrator (SecurityAdmin) user account.
- Open Cybersecurity Admin Expert.
- Select ROLES tab > SECADM role.
- Expand CAE item in the Permissions area.
- Enable Model Management and Model View:
- Click Save changes. The MODELS tab is added.
Adding, editing, or deleting a model
Default models are predefined and cannot be edited.
- Open Cybersecurity Admin Expert.
- Select MODELS tab:
-
Add model: click Add model button, edit details.
-
Edit model: select a model and edit details.
-
Delete model: select a model and click the Trash icon. SAM model can not be deleted.
- Click Save changes.
Adding or editing model Permissions, Objects, Actions, or Parameters
- Open Cybersecurity Admin Expert.
- Select MODELS tab > select a model:
-
Add or edit Permissions: click Add permission or select a permission and click Edit permission.
-
Add or edit Object: select a permission and click Add object or select an object and click Edit object.
-
Add or edit Action: select an object and click Add action or select an action and click Edit action.
-
Add Parameter for DSS: scroll down and click Add Parameter. You can set specific security parameters by model, such as disabling a USB port or WI-FI access.