Editing a Component
Edit a component when you want to reuse a number of its properties. You can then save the edited version under a different name or in a different category.
Changes to a custom component are applied to the same component used in other pages.
Editing the <Component> definition from within the TGML document is not supported. For more information on editing components, see Adding custom components.
To edit a component:
- Open Graphics Editor.
- Components pane > select a category.
- Right-click the component > Edit.
- Edit the component.
- File > Save As > click Component.
- Select the category you want.
- Click OK.The Properties dialog box opens.
- Enter a name and description.
- Enter the Height and Width of the component.
- Click OK.