Grouping Drawing Objects as a Component
Group multiple drawing objects within a graphic as a component for bind naming and graphics design efficiency. In order to save your work to a components library for reuse, the drawing elements must be grouped as a component.
NOTE: Any advanced one-line components of the same type (e.g. Breaker) with the same Name attribute value will animate identically.
To group drawing objects as a component:
- In Graphics Editor, in the Layers pane, select the layer that contains the drawing objects you want to group.
- On the work area, select all drawing objects that you want to group as a component.
- Right-click the selected objects, point to Group as, and then click Component.
- On the File menu, click Save.