Adding a Linear Gradient
You add a linear gradient to give an object a smooth, varying hue from one point to another.
For more information, see section the Gradients Overview section.
To add a linear gradient:
- In Graphics Editor, in the work area, select the object on which to apply the gradient.
 - On the Options toolbar, click Fill to open the Color/Gradient palette.
 - Click the Gradient tab.
 - Click the box with the gradient you want to use.
 
In the Objects pane, a LinearGradient element and two or more GradientStop elements are added to the object.