Editing a Text Path
You edit a text path to change its appearance or other properties. The text path is in fact a curve and can be modified like any other curve, but you can no longer edit the text itself.
For more information, see the Adding Text and Textboxes section.
To edit a text path:
- In the Properties pane, edit the properties (Fill, Opacity, Stroke, StrokeDashArray, StrokeWidth, or Visibility).
- Double-click the path and drag the vertices to change the shape of the path.

- Click outside the textpath to clear the selection.
In Graphics Editor, in the work area, select the text path.