Skewing Objects
Skewing an object means that you distort the shape in a horizontal or vertical direction by a number of degrees. You skew by selecting one or several objects and then applying a value from the horizontal or vertical skewing menu.
You skew horizontally to transform an object along the x-axis. The skew angle is measured in degrees from the y-axis. You skew vertically to transform an object along the y-axis. The skew angle is measured in degrees from the y-axis.
To skew horizontally or vertically:
- In Graphics Editor, in the work area, select the object you want to skew.
- On the Options toolbar, click the Skew Horizontal button
or the Skew Vertical button
to open the degree selection menu. - Click the required amount of degrees, –60° to +60°.
NOTE: A positive value implies counter-clockwise skew. A negative value implies clockwise skew.