Drawing a Polygon
Use the Graphics Editor Polygon tool to draw a polygon, that is, a plane figure that is bounded by a closed path, composed of a finite sequence of straight line segments.
You draw a polygon when you need a closed multi-sided figure.
To draw a polygon:
- In Graphics Editor, in the Layers pane, select the layer where you want to draw the polygon.
- On the Drawing toolbar, click Polygon.
- In the work area, click where you want to locate the corners of the polygon.

- Double-click to close the polygon.
- On the Drawing toolbar, click Select.
- In the Properties pane, in the Name box, type the name of the polygon.
NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.

- On the Options toolbar or in the Properties pane, adjust the appearance of the polygon.
- On the File menu, click Save.