Drawing a Rectangle
Use the Graphics Editor Rectangle tool to draw a simple rectangle, that is, a quadrilateral with four right angles.
You draw a rectangle when you need a four-sided figure with four 90° angles and there is no component that works for this situation.
For more information, see the Drawing Tools section.
To draw a rectangle:
- In Graphics Editor, in the Layers pane, select the layer you want to draw the rectangle on.
- On the Drawing toolbar, click Rectangle.
- In the work area, click where you want the rectangle to begin and drag the pointer to where you want it to end.

- On the Drawing toolbar, click Select.

- In the Properties pane, in the Name box, type the name of the rectangle.
NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.

- On the Options toolbar or in the Properties pane, adjust the appearance of the rectangle.
- On the File menu, click Save.