Supported File Formats
Create graphics in Graphics Editor using TGML or SVG files converted to TGML.
It is not recommended to insert pictures using common image file formats such as JPEG or PNG, due to the lack of resolution when zooming, but more importantly because it will negatively affect performance of the WebHMI for the operator by creating large graphic file sizes.
Graphics can be exported to common image file formats, including JPEG, PNG, and Bitmap for example.
You can import other graphics or photographs in supported formats. The following formats are supported Editor:
| Graphic Type | File Type |
|---|---|
| Bitmap | .bmp, .dib |
| GIF | .gif |
| JPEG | .jpg, .jpeg, .jpe, .jfif, .exif |
| PNG | .png |
| TIFF | .tiff, .tif |
| Icon | .ico |
| Metafile | .wmf, .emf |