Graphics Editor Binds and Links Pane
Use the Binds and Links pane to get an overview of the binds and links used in a graphic and their properties.
NOTE: The actual binding and linking are performed in the Graphics Editor.
                                            
                                        
| Component | Description | 
|---|---|
| Name | 
                                                         Displays the name of the bind/link, consisting of the object’s name and, for the binds, a suffix normally ‘Value’. Name also shows the number of bind values or link targets that use this name. (One signal can affect several properties.)  | 
                                                
| Attribute | 
                                                         Displays the property (if present) that is affected by the bound value.  | 
                                                
| Format | 
                                                         None or Presentation. As selected in the Properties pane, under Behavior - Format.  | 
                                                
| Description | 
                                                         Displays an optional descriptive text.  |