Graphics Editor Options Toolbar

Use the Drawing toolbar to access the tools you need to create and edit .tgml files and other objects.

Button Description

Point Selection
Click the border, or anywhere within a filled object, to select the object and display the curve points.

Rotate Selection
Click to rotate the selected object by dragging the handle that is displayed at the top of the object.

Fill

Select the required fill color or gradient from the palette.
For more information, see the Gradients Overview section.

Swap Colors
Click to swap the current colors of the stroke and the fill.

Stroke

Select the required stroke color or gradient from the palette.
For more information, see the Gradients Overview section.

Style

Select the required stroke style from the list.

Width

Select the required stroke width, 0–30 pixels, from the list.

Corner

Select the required corner radius, 0–50 pixels, from the list.

Group
Click to group the selected objects in the work area.

Ungroup
Click to ungroup objects that were previously grouped.

Arrange
Select the required arrangement of an object relative to other objects, from the list.

Distribute
Select the required distribution of three or more objects, in the horizontal or vertical direction, from the list.

Flip
Select the required flip operation of the selected object, in the horizontal or vertical direction, from the list.

Resize
Select the required resize operation of two or more objects from the list: same width, height, or width and height.

Rotate Left
Click to rotate objects (single or group) 90° left.

Rotate Right
Click to rotate objects (single or group) 90° right.

Skew Horizontal
Click to skew the objects (single or group) horizontally to ±60°, ±45°, ±30°, or ±15°.

Skew Vertical
Click to skew the objects (single or group) vertically to ±60°, ±45°, ±30°, or ±15°.

Font
Select the required font family from the list.

Size
Select the required font size, 8–100 pixels, from the list.

Bold
Click to make the characters of the selected text string or text box bold.

Italic
Click to make the characters of the selected text string or text box italic.

Underline
Click to make the characters of the selected text string or text box underlined.

Strikethrough
Click to display the characters of the selected text string or text box with strikethrough.

Text Align Left
Click to align the text to the left based on the insertion point of the text row.

Textbox Align Left
Click to align the text to the left in the text box.

Text Align Center
Click to center the text based on the insertion point of the text row.

Textbox Align Center
Click to center each text row in the textbox.

Text Align Right
Click to align the text to the left based on the insertion point of the text row.

Textbox Align Right
Click to align the text to the right in the text box.

Text Align Top
Click to align the top of the text to the insertion point.

Textbox Align Top
Click to align the text to the top of the textbox

Text Align Middle
Click to align the middle of the text to the insertion point.

Textbox Align Middle
Click to align the text in the middle of the texbox.

Text Align Bottom
Click to align the bottom of the text to the insertion point.

Textbox Align Bottom
Click to align the text to the bottom of the textbox.