Unsupported Characters
Object names cannot include any of the following characters: exclamation point (!), quotation mark (“), number sign (#), percent sign (%), ampersand (&), apostrophe ('), left parenthesis ((), right parenthesis ()), asterisk (*), plus sign (+), comma (,), hyphen-minus (-), semicolon (;), less than sign (<), greater than sign (>), equals sign (=), question mark (?), backslash (\), or pipe symbol (|).
In addition, the following restrictions apply:
- Object names can contain spaces, however, leading and trailing spaces are not supported in objects names.
- Object names can contain full stops (.), however, leading and trailing full stops (.) are not supported in object names.
- Object names cannot be empty names.