Installing Graphics Editor
Graphics Editor is automatically installed with Power Operation, provided that the Configuration and Development Environment option is enabled on the Core Components page of the installer. It is recommended to install Graphics Editor when installing Power Operation because its major features are interconnected. However, Graphics Editor can be installed and uninstalled independently. In the event of abnormal behavior within Graphics Editor, uninstall and then reinstall Graphics Editor.
To install Graphics Editor:
- In
...Power Operation/setup/Installers/GraphicsEditor, right-click Graphics Editor and select Run as Administrator from the context menu.
To uninstall Graphics Editor:
- In Windows Control Panel, navigate to Programs and Features.
- Right-click Graphics Editor, and then, from the context menu, select Uninstall.
OR
- Open Graphics Editor. The Program Maintenance page of Graphics Editor installer will open.
- Click Remove.
For more information, see Learn more about Graphics Editor installation.