TGML Format Specifications
Additions to the TGML Format Specification:
TGML Appendix A: User-Defined Descriptions of Custom Attributes
In Graphics Editor, when an attribute is selected, a short description of the element attribute is displayed in the properties pane.
Custom attributes have no description since the TGML implementation has no knowledge of the attribute. However, it is possible to use Metadata to add a description of a custom attribute:
Example TGML code containing a user-defined description of a custom attribute. When the user selects MyAttribute in the Graphics Editor properties pane the description is displayed:
<TGML>
<Component Left="100.0" Top="100.0" Width="30.0" Height="30.0" ContentWidth="30.0" ContentHeight="30.0" MyAttribute="0" >
<Metadata Name="MyAttribute" Value="This is a description of MyAttribute"/>
.
.
.
</Component>
</TGML>
The Name of the Metadata element has to be the same as the attribute name. Value contains the description.
TGML Appendix B: TGML View Object
Appendix B describes the TGML JavaScript Global Objects, the TGML View Object, and the TGML Console Object.
TGML JavaScript Global Objects
| Global Object | Description |
|---|---|
| view | The view object |
| Console | The console object |
TGML View Object
| Members | Description |
|---|---|
| document | The document object |
| width | Width in normal pixels |
| height | Height in normal pixels |
| zoomLevel | Zoom level, a floating point value where1.0 is no zoom, <1 is zoomed out, >1 is zoomed in. |
|
touchEnabled |
Touch device (true/false) |
| addEventListener(type, listener[, useCapture]) | Adds an event listener. Supported event: ‘resize’. See w3c standard interface EventTarget |
| removeEventListener(type, listener[, useCapture]) | Remove an event listener. Supported event: ‘resize’. See w3c standard interface EventTarget |
Example: The view properties are displayed in a textbox and updated when the viewer resizes or the zoom level changes:
<TGML>
<TextBox FontFamily="Arial" FontSize="15" FontStyle="Normal" FontWeight="Normal" Height="30" HorizontalAlign="Center" Left="0" Name="" Opacity="1.0" Stroke="#000000" TextDecoration="None" Top="100" VerticalAlign="Middle" Width="200">
<![CDATA [width/height@zoomLevel]]>
<Script OnDocumentLoad="load"><! [CDATA [
function load(evt)
{
function updateView()
{
evt.getCurrentTarget().setAttribute("Content", view.width + 'x' + view.height + '@' + view.zoomLevel + (view.touchEnabled ? ' touch' : ' mouse'));
}
view.addEventLister('resize', function () {
updateView ();
});
updateView();
}
]]>
</Script>
</TextBox>
</TGML>
TGML Console Object
| Members | Description |
|---|---|
| info(obj1 [, obj2, ..., objN]) | Outputs a message to the Console view |
| warn(obj1 [, obj2, ..., objN]) | Outputs a message to the Console view |
| error(obj1 [, obj2, ..., objN]) | Outputs a message to the Console view |
| log(obj1 [, obj2, ..., objN]) | Outputs a message to the Console view |
Example: Outputs the message “test 9” to the console view:
<TGML>
<Script OnDocumentLoad="load"><! [CDATA [
function load(evt)
{
console.log('test', 9);
}
]]></Script>
</TGML>