TGML Grouping: <Group>
The Group element is a container element, used for grouping elements together so they can, for example, be moved, copied and resized as if they were a single element.
| Attribute | Type | Description |
|---|---|---|
|
Opacity |
Double |
A value between 0.0 (transparent) and 1.0 (opaque). |
|
Visibility |
Visibility |
Specifies if the element shall be visible or not. |
Example:
Copy
<TGML>
<Group Opacity="0.5">
<Line Xl="50.0" Yl="50.0" X2="l50.0" Y2="150.0” />
<Line Xl="50.0" Yl="100.0" X2="150.0" Y2="200.0" />
</Group>
</TGML>