TGML Polygon
The <Polygon> element describes a polygon, which is a connected series of lines that forms a closed shape. The end point does not have to be specified. The polygon is closed automatically.
| Attribute | Type | Description |
|---|---|---|
|
Fill |
Brush |
Specifies how the interior of the shape is painted. |
|
Opacity |
Double |
A value between "0.0" (transparent) and "1.0" (opaque) |
|
Points |
Array of Point |
The vertex points of the polyline: |
|
Stroke |
Brush |
Describes how the line is painted. |
|
StrokeDashArray |
Array of Double |
The pattern of dashes and gaps used to outline shapes: |
|
StrokeWidth |
Double |
The width of the outline of a line. |
| Visibility | Visibility |
Specifies if the element is visible or not. |
Example:
<TGML>
<Polygon Points="50.0,150.0 100.0,50.0 150.0,150.0" Stroke="#0000FF" Fill="#FFFF00"/>
</TGML>
Example on screen: