TGML Standard DOM Methods (Commonly Used)
The following is an overview of standard DOM methods that can be used to access graphics elements and attributes.
See W3C Document Object Model (DOM) Level 3 Core Specification for more information.
| Object | Method | Description |
|---|---|---|
|
Any element |
getAttribute("‹attribute›") |
Returns the value of ‹attribute›. |
|
Any element |
getChildNodes() |
Returns a NodeList that contains all children of this node. |
| Any element |
getOwnerDocument() |
Returns the document. |
| Any element |
getParentNode() |
Returns the parent element. |
| Any element |
getTagName() |
Returns the element tag name, e.g. Rectangle or Bind. |
| Any element |
setAttribute("‹attribute›", "‹value›") |
Sets the value of ‹attribute› to ‹value›. If the element does not have the attribute, it is created (as a TGML custom attribute). |
|
Document |
getDocumentElement() |
Returns the TGML (root) element. |
| Document |
getElementById("‹Id›") |
Returns the child element that has the Id attribute with the given value. |
| Document |
getElementsByTagName ("‹tagName›") |
Returns a NodeList of all the elements in document order with a given tag name. |
| NodeList |
getLength() |
Returns the number of elements in the NodeList. |
|
NodeList |
item("‹index›") |
Returns the element at ‹index› in the NodeList. |
Example:
<TGML>
<Rectangle Left="50" Top="50 Width="100" Height="100" Fill="#C0C0C0" Stroke="#000000">
<Script OnMouseOver="over" OnMouseOut="out"><![CDATA [
function over(evt)
{
// Change fill color while hovering
var rectangle = evt.getTarget();
// Get the original fill color and store it
// as a custom attribute of the rectangle
var color = rectangle.getAttribute("Fill");
rectangle.setAttribute("originalColor", color);
// Change the color to blue
rectangle.setAttribute("Fill", "#0000FF");
}
function out(evt)
{
// Restore the fill color
var rectangle = evt.getTarget();
var color = rectangle.getAttribute("originalColor");
rectangle.setAttribute("Fill", color);
}
]]></Script>
</Rectangle>
</TGML>